Other Parts Discussed in Thread: BQ34Z100
I have a 11Ah 10s battery, using bq34z100 as a FG. The battery has three operation modes:
- normal operation - charge with up to 4A or discharge with up to 20A current everything looks ok
- standby - battery is off, but the microprocessor is operational for an hour, before going to low power mode - BMS draws about 15mA
- low power mode - after an hour of inactivity, the battery goes into deep sleep mode with only 300uA being drawn by the BMS
The problem is, that the SoC reduction reported by the FG when the battery is in low power mode is not accurate - it looks like the FG still reads the standby current of 15mA and in a matter of 10 days the SoC drops by 15-20% although the actual capacity has not. Resetting the FG brings the SoC back to normal.
My guess is that the standby current is not measured correctly, but since the CC Offset is calibrated automatically I do not see how to overcome this issue. I have checked that it is changed from the value of the golden sample and it is in fact. My question is, is it possible that it is done during the standby mode of 1 hour and once the battery goes into a low power mode, the error is significant enough to introduce wrong reading over the time of the coulomb counter?
I am trying to attached a gg file but unfortunately don't see how.
Any advise is appreciated.
Regards,
Peter Marinov