I plan to use the LMZ13610DEMO board to create a constant current supply by tinkering with the feedback from an external current sense resistor. When the load is removed, the LMZ13610 will have no feedback to control the output voltage. Will this damage anything? My normal load will be 2VDC to 6VDC, so input voltage can be 12VDC.
Ron