This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

srec not matching error msg. when using ev2400 to program bq78350 on bq76930evm

Other Parts Discussed in Thread: BQSTUDIO, EV2400, BQ76930EVM, BQ78350

I have received the EV2400 and it does seem to communicate with bqStudio software.

I am trying to use this along with the bq76930EVM.

 

When trying to program the srec file for the bq78350 gas gage IC, I see a message from the bqstudio stating that EV2400 may have issues and I may need to use the EV2300?  Also on using the Firmware program feature , the srec file does get programmed but I get back an error stating that the check sum of the srec files does not match.

 

 

Wondering if this is a known issue and do I need to switch to EV2300 OR is there  a way to use the EV2400  with the bq78350 and bq76930EVM?