Can you tell me what the turn-on and turn-off drive currents are for the bq769x0 DSG and CHG outputs?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
See the "Charge and Discharge Driver" section of the datasheet. The outputs have different resistances for on and off.
Turn on can be calculated from the rise time and should give ~5k ohm, so nominal maximum drive current is when the outputs are low and would be 12/5k or 2.4 mA.
Turn off is different between the outputs and the pull down resistance is shown in the datasheet, 1M nominal for CHG and 2.5k for DSG
The turn on will be an exponential charging the load capacitance (FET gate capacitance) through the (DSG) pin drive output source resistance. The current is the "high" 2.4 mA when the voltage is at 0 and very small when the voltage is near final voltage.
For a high capacitance gate or a FET array with high capacitance you will need a FET driver external to the bq769x0. You might look at www.ti.com/lit/ml/slup169/slup169.pdf or information from your preferred FET supplier. Be aware that the bq76930 and bq76940 generally do not tolerate long propogation delays for the driver to act since the power pins can be pulled down by a very heavy load such as short circuit. The SC delays are relatively short, so these parts will work best if your FET switches moderately fast after a short propogation delay, or if your system turn on has a current limit or soft start function. If it is suitable, your system might also be able allow a SCD trip or more at turn on to "charge" the system, but be careful of FET heating and differentiate between a normal turn on and a turn on into a short.
Of course also be cautious of switching too fast and creating an inductive response in the cells