This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65910A3 START UP PHASE WITH VRTC

Hi my Customer BM is using the TPS65910a3 and he connect the VRTC to PWRHOLD.

PWRON is connected to VCC7 and to the input VCC 5V.

PWRHOLD is connected to VRTC.

The question is: what happen at startup when VCC 5V is active?

will VRTC be active after supplyng VCC7?

i can also provide you the sch for review...

Regards,

kamal