I have been testing the threshold for the VBAT_OK threshold and what I am seeing is that I have programmed for a descending voltage a threshold on VSTOR 2.336V and I am watching it trip at different voltages each time I tested it. I saw a trip voltage of 2.680V, 2.607V and then 2.404V remember my trip voltage is (2.336V). I am bleeding off the SEC_STORAGE with a 16mA resistive load and measuring the voltage with a scope. On the VBAT_OK_HYST I had programmed value of 2.68V for the ascending voltage. I have since tested this three times and I am seeing a voltage of 2.81V, 2.691V and 2.683V my programmed value was a(2.680V). What I am trying to find out is if this is a normal expected variation in the VBAT_OK threshold and if so what would the max/min variations over temperature.