My customer has questions on the BQ40Z50 based uponthe application schematic shown in Section 5.2 of the bq40z50EVM Li-Ion Battery Pack Manager Evaluation Module User's Guide, SLUUAV7 - December 2013.
1. Our standard external PTCs have a nominal resistance of 100K. We would like to know if it is possible to use them at locations RT2-5.
2. We do not have a System Present signal on our battery packs. What would the implication of having this signal permanently tied to ground through a 10K resistor be?
3. If the LEDs are to be used, should the pin LED* be tied to ground? The datasheet refers to grounding this pin when LEDs are NOT used, while the EVM schematic shows a push button that grounds that pin momentarily in order to get the LEDs to light up.
4. Some protection elements are drawn on the schematic right next to J4. What are they?
5. Can you suggest chemical fuses rated for 30A, other than the Dexerials (formerly Sony)? Do you have a contact at Dexerials? We sent a couple of website messages to them that have not been answered yet...
6. What shunt value do you recommend for a +/- 50A or 60A current measurement range?
7. Do you have a recommended solution for a Bluetooth Smart (or BLE) IC that can interface to the bq40z50? Should we decide to implement such a solution, we would have to power it through a DC-DC regulator from the stack, as the bq40z50 does not feature an external power feed, correct?
8. Is there a way to "wake up" the bq40z50 from a device or system sleep mode in hardware (such as changing the level of a pin, or sending an SMBus signal)?
9. Are there internal pull-ups on the SMBC and SMBD ports or do they need to be provided if the bq40z50 is a master? Shall we assume that the charger may have them?
Thanks,
John Porter