This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65136 as bipolar low-current audio supply

Whilst I'm aware that this is not its intended purpose I'm using the TPS65316 as a bipolar supply for a low-power audio stage in high-fidelity portable application where noise performance is very important.

The datasheet suggests that if the current draw on either of the outputs differs by greater than 30%, the device will go out of regulation.

Under high output levels, the audio drive current will be the dominant draw on the device and I believe this will indeed lead to a greater than 30% difference between the positive and negative rails. This mismatch will be following the audio signal (e.g. reverse at a frequency of no less than 20Hz) and the overall current draw will be considerably less than the total ability of the device.

Does the AC nature of the current draw mitigate the current mismatch between the rails?
Is 30% still a relevant figure for the device going out of regulation if the total current draw is less than, say, 100mA.
Do you have any suggestions as to how prevent the device going out of regulation in this application, or do you feel the part is entirely unsuitable - if so, can you recommend another solution with similar output noise characteristics and minimal external component count?

Regards,

Sam.

  • Hello Sam,

    In general the part can overcome the mismatch of some mA with an integrated circuit. In addition, you can minimize the AC load by increasing the output capacitance.

    So the only possibility to be sure if the part can work in this application or not is to test it. Sorry, but due to the fact that the mismatch is not really known, it is not possible to give here a definitive answer.

    Best regards, Brigitte

  • Dear Brigitte,

    Thanks for your response.

    To confirm - there is no specific data available regarding the acceptable mismatch before regulation fails, other than the 30% figure quoted in the datasheet?

    Regards,

    Sam.

  • Hello Sam,

    You are right, there is no specific data on when exactly the part stops operation due to load current mismatch. It was tested that the part can work with 30% mismatch, but not when exactly it stops operation above 30%.

    BTW, you are aware that the positive output has a fixed voltage of 4.6V?

    Best regards, Brigitte