hi,
today i tried to set cell balance e.g. CELLBAL1 set to 0x03, CELLBAL2 and CELLBAL3 set to 0, on monitoring these cell voltage i don't see voltage drop across these cells, because the DEVICE_XREADY flag is 1 ?
cheers,
Tiger
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
From what I understand only the BQ76920 has built in cell balancing, your model requires external components to do the actual balancing.
It sounds like you got some sort of Permanent Fail that caused the XREADY bit to be set. If the XREADY is set.
In page 26 of the bq76930 Datasheet, there is a note that says the following:
"NOTE
All cell balancing control bits in CELLBAL1, CELLBAL2, and CELLBAL3 are automatically
cleared under the following events, and must be explicitly re-written by the host
microcontroller following clearing of the event:
• DEVICE_XREADY gets set
• Enters NORMAL mode from SHIP mode"
-Francis H