The LM25011 datasheet states on pg 15, just below equation 8 that "For this example, RFB2/RFB1 = 0.992. RFB1 and RFB2 should be chosen from standard value resistors in the range of 1.0 kΩ – 10 kΩ which satisfy the above ratio." No explanation is given as to why this limited range is necessary.
When WEBENCH is fed the values, 8 < Vin < 36, Vo = 5V at Io = 1.5A, as per the datasheet example, it chooses feedback resistors within the datasheet specified range.
However, when WEBENCH is given the parameters 12 < Vin <14, Vout = 9V at I = 1.3A, it chooses Rfb1 = 9.76k and Rfb2 = 25.5k. The latter is well outside that which the data sheet range.
Is the datasheet wrong, or is WEBENCH wrong?