This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65910A31 and AM3352 condition in Power OFF and next POWER ON state and RTC only mode



Hello,

We are designing a portable device for which we have  selected TPS65910A31  PMIC for AM3352  so that VDDS_RTC can be directly sourced from VRTC of the PMIC. I have connected a 3.1V Coin battery to VBACKUP of PMIC and also have connected  INT1 and SLEEP of PMIC to the processor.. I have  a query

1.Our portable device rely on processor RTC for DAY/MONTH/YEAR and HOUR/MINUTE/SECONDS information.

Will the RTC keeps running irrespective of Power ON and OFF condition  of the processor and the PMIC.

kindly provide me the information.

Regards,

Mamatha