Hi everyone,
Attached is a schematic of our BQ24650 design for a lead-acid battery along with some debug notes. Note that we have fixed the location of R98 (now connected to anode of D12 instead of gate of Q5). We had seen this design working in lab (charge currents up to ~500mA). However, when we took it in the field to test, we found that all of a sudden the charge current from the solar panel was only around 20mA and that the battery voltage was slowly dropping as it wasn't charging.
Bringing the board back into lab, I tested it exhaustively and found that we have a FAULT condition (both LEDs unlit) and that we immediately enter termination (Vfb > Vrech) when Vcc > 0V (solar charging is connected). We aren't hitting the first 3 fault conditions listed in the spec: temperature suspension, over voltage or sleep. We may be hitting battery absent, since it sounds like the test is similar to checking for termination, but that would just point back to the termination issue.
I've also checked for all the conditions outlined in the 'Enable and Disable Charging' section of the spec (p. 14), and we aren't meeting any of the conditions. The only one I'm unable to check is the TSHUT IC temperature, which I'd need to find a way to check.
My primary questions are:
1) Given the same battery voltage at the output node of the charger, how could Vfb jump from 1.895V (not in termination) when no solar charging is applied (Vcc = 0V) to 2.05V (termination) when solar charging is active (Vcc > 0V)?
2) Are there any other additional conditions that cause a FAULT other than the 4 listed in the spec?
3) How can we test if we have hit the TSHUT IC temperature?
We now have a second board running in the field flawlessly, so I'm a bit concerned why the first board should fail. Before I call the IC dead, I wanted to ask your help.
Let me know your thoughts.
Thanks!
Matt