Hello all:
I'm using the TPS73433 regulator in my circuit. I'm wanting to add more load which would exceed this regulator's 250mA capacity. Would it work to use two or more of these in parallel to increase current-handling capacity? I know there's a 500mA version of this part, but only available in SON package -- I'm hand-soldering, so can't use it.
If using more than one in parallel would work, can they share capacitors, or would each regulator need its own set?
Perhaps this is a naive question, but I had to ask. :-)
-Mike