Hello.
I feel confused about the different duty cycle between UC3843 and UC3844 . Can you tell me where I must use the 50% duty cycle (UC3844) ,and where I must use the 100% duty cycle (UC3843) ?
I want to use UC3843 in my new product . Will you please tell me is it suitable for my require? Some detail information as follows:
1. Vin = 18 V DC to 36 V DC
2. Vout1 = 15V , 100mA.
3. Vout2 = 5V, 2000mA
4. efficiency =70%