Hi,
We are using the bq24251 in a new product but would like to decrease the battery recharge time. At present we have set the ILIM value to about 1.5A and the ISET limit to about 1A but cannot obotian an input current greater than about 800mA. I can get up to 900mA - 1A or so by increasing the input voltage to about 5.6V, but at the 5V we are using I only get the 800mA. I have changed the system load and can reduce the charge and/or input current using software settings but still hit the 800mA input limit.
I have also shorted out the ILIM resistor, again without improvement.
I have looked at and tried alternative inductors in case I am hitting a saturation problem, although I don't think this should effect the input limit.
The charger is being reported as a SDP type, but, again, I've tried different types without improvement.
Any other ideas as to what the problem could be?
Thanks,
Richard Prosser