Hi,
My customer has TPS3808G01 implemented in several designs. On occasion, the TPS3808G01 will hold /Reset active and keep it there, even though the criteria for releasing /Reset have been met. My customer claims that washing the circuit board fixes the problem. Here is my customer's description of the problem:
Here’s an example of one of the circuits we have (This circuit is not the only one that causes problems, however.):
(NOTE: I pointed out that the schematic does not show a 10nF cap on the SENSE input. Customer has since added the cap; no change)
The two outputs, RSMRST~ and PWR_BTN~ feed directly into the Via CX700 system processor. I have measured and verified that the MR input is at 3.3v, the VDD power rail is 3.3v, the SENSE pin is over 0.405v (usually between 0.480 and 0.6v depending on the specific circuit). On one of my boards I have also disconnected R147 and R572 to see if somehow loading is causing the problem, and the reset still doesn’t go high.
On another board, with a different circuit using the TPS3808, the RESET~ output feeds into two IC’s (a 7400 series AND gate and a Multivibrator Reset input). I found that if I disconnected both loads the 3808’s reset would finally drive high. This shouldn’t be the case because both inputs are high impedance. Perhaps there’s some capacitive load requirement the 3808 spec doesn’t mention?
Are there any known problems with TPS3808?
Thanks,
Rick Rubio