Hi,
Can some one help me understand why the when I design the evaluation board spec TPS402101EVM with switch pro the values are different from those of actual TPS40210EVM board. For example the inductor used in EVM board is 10uH whereas that suggested in switch pro design is 1uH.
IF I follow the datasheet the values comes different from the switchpro design, do I need to make any adittional consideration than given in the datasheet for calculating especially for inductor.