Other Parts Discussed in Thread: BQ51050B
Hello,
I've some struggles with my bq51050b design.
Here is my schematic diagram:
(Values of serial and parallel capacitors in receiver resonance circuit are only illustrative. Actual values were adjusted to the inductance of my RX coil.)
When I place the receiver over the transmitter pad, I get VRECT around 8 Volts. However, it is interrupted every about 10 seconds. Here is the waveform:
Moreover, the receiver fails in starting the charging sequence. Output voltage is zero, weather the battery is connected or not. (My battery is 300 mAh with 4.2 V charging voltage and desired charging current around 150 mA)
I'd appreciate any suggestions.
Thanks
Pavol