We use the TPS65950 (PMU) with an OMAP2. When our unit is "off" VBAT=2.8 to 3.0V (PMU is in Wait-On state). When we apply power
VBAT rises to 4V and the "START_ON VBAT" event starts the PMU. This works most of the time.
These two conditions seem to prevent or not allow the "START_ON VBAT" event to start the PMU (Wait-ON to active).
Condition one:
If we write the DEVOFF bit to the PMU to shut off. (VBAT=3V and in Wait-on state) The next time we apply power, the PMU does not
turn on when the VBAT voltage rises to 4V? And yes we have that starting event enabled.
Condition two:
Our unit is off and VBAT=3V. We connect a USB cable to the unit and then disconnect the USB cable. (The unit is still off). The
next time we we apply power, the PMU does not turn on when the VBAT voltage rises to 4V?
Does anyone know why either of these conditions prevent the PMU from starting up from the "START_ON VBAT" event?
Thanks,
Tony Wilkey
RELM Wireless.