Assuming I follow the rules in the datasheet, the LMZ14203H is EMI certified for radiated emissions without external filters and is EMI certified for conducted emissions with an external LC filter when operated in "normal" mode with Vin = positive and Vout = positive. However, I want to use the LMZ14203H in inverting mode with Vin = positive and Vout = negative.
Based on the internal topology of the IC, what EMI changes, if any, can be expected from using inverting mode.
Also, does anyone have experience with their product passing EN 55022 Limit (Class B) while using an LMZ power module in inverrting mode.
Thank you
Ed