This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

bq25504

Other Parts Discussed in Thread: BQ25504, TPS61020, TPS3839

Hello,  Dear TI support,

in bq25504 data sheet, "Battery Status output - can be used to enable or disable system loads" what is this mean.

also at Page 14, 8.4.2 Main boost Charger enabled (...) and EN# = LOW,

where is this EN#.

I will use this chip as a back up booster only when the battery goes lower than 0.9V, there is another booster(TPS61020) in parallel

with bq25504, in default mode, TPS61020 works, bq25504 disabled. if the voltage is lower than 0.9V, ( TPS61020 disabled).

then bq25504 start to work to use the rest of the engineer in the battery. I hope to put this chip in disable mode to consume as less

power as possible. couldn't figure out how to control it.

thanks,

David