Hi
I'm interested in building an MPPT battery charger capable of charging 12/24/36/48 volt batteries from an input voltage between 3v ~ 48v.
I intend using the SM3320-BATT-EV and AN-2178 as reference designs. Can anyone advise what changes are recommended to these reference designs to achieve the above? For example, in AN2178 where a LM5118 is used, what size should I make L1 and the MOSFETS to achieve a higher output voltage and whether there are any other hardware changes to consider?
I am very amateur at this and would appreciate any advice given.
Kevin