This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Using More than one External Temp Sensor on a BP76920+BQ78350

Other Parts Discussed in Thread: BQ78350, BQ76920, BQ40Z50, BQ76930

From customer:

Can you please find out if there is any way of getting more than one external temperature sensor on a bp76920+bq78350 - based solution? This is very important to us. If the answer is no, we'll be forced to choose between a bq40z50 (which does not scale up to 8, 12, and 15 cells) or a bq76920+ ARM or MSP430 solution with the SOC and additional temp sensors would be monitored.  It would also be good to know if using a 76930 for a 4-cell solution (which would give us a second external temp sensor) is supported by the bq78350...