Dear Sir
Good days,
Due my customer system load may over 8A ,so we want set up input current limit is around 16A.
the question 1 is if we want to set up input current limit is 16A, we just set Rac from 10m ohm to 5m ohm?
the question 2 is if we set Rac = 5m ohm,then how to set up DS table 6?(for example if the "Input Current, DACIIN 0" bit will be "0"=Adds 0mA of input current "1"=Adds 256mA of input current)
Best regards,
Bogey