I have read that charging Li ion battery has some particular algorithm:
1)Charge at constant current (0.2 C to 0.7 C depending on manufacturer) until the battery reaches 4.2 Vpc (volts per cell),(70% cell is charged)
2)Hold the voltage at 4.2 volts until the charge current has dropped to 10% of the initial charge rate. The termination condition is the drop in charge current to 10%.
But this type of charging cant be followed with BQ25504EVM,
So is that I wont be able to charge a battery completely to 100% SOC(state of charge)?
Li ion charging algorithm: