This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Differences between the Webench board layout and Skematic for LM25085

I am working on integrating this circuit into a larger PCB using EagleCad Pro V 7.1.0

Using the Webench tool export function, I have been able to successfully download, both the schematic and the board layout to eagle, However when I try and merge the schematic and the layout, there are several consistency errors, revolving around various components missing from the schematic file.

What are these extra components? Is it normal for the provided schematic from the Webench and the provided layout to be inconsistent? And is there anything I can do to avoid this issue, or do I need to solve each conflict manually in Eagle?