When the BQ78350 wakes up from sleep mode, can it be configured to automatically turn on the DSG and CHG outputs?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
When the BQ78350 wakes up from sleep mode, can it be configured to automatically turn on the DSG and CHG outputs?
Hi Jessica,
The CHG FET behavior in sleep mode is configurable by setting or clearing the DA Configuration[SLEEPCHG] flag. Just search for SLEEPCHG in the TRM.
For the DSG FET, there is no configuration but behavior depends on how sleep mode was activated. If sleep mode is entered by the gauge - that is the rules for going to sleep are valid, then the DSG FET will remain on. However, if you issue the MAC command 0x0011 to enter sleep, then the DSG FET will be turned off. Reference section 16.2.11 in the TRM.
Regards,
Doug
Thank you for the clarification.
I'm still a little fuzzy on how one would "reset" the device after a sleep event or an error event. Is toggling the KEYb in line the typical way to turn a circuit back on? Will that work to clear error events, or does MRSTb need to be toggled for that?
Hi Jessica,
When KEYIN is asserted, a timer starts. If the time is exceeded then DSG FET is turned off. Then, when KEYIN is deasserted the DSG FET is turned back on again. The polarity of the assert/deassert may be changed.
If the chip is in SLEEP, the KEYIN line works the same way.
Regards,
Doug
Hello Doug,
Thank you for further clarifying the behaviors for us. We appreciate the quick responses!
Best,
Jess