Hi,
I want to use BQ24257 in standalone mode, so without using I2C..
I see that for setting the value of the fast charging current I need to connect a resistor on the ISET pin.
this pin have a minimum RISET value of 75 Ohm but it don't specify a maximum value so I theorically set fast charging current at very low value but on the electrical characteristics I found the information that the fast charging current can only be set between a value of 500mA to 2A.
So my question is: what limit the minimum fast charging current at the value of 500mA? there is no possibility to set the fast charging current at lower value with standalone mode?
Thanks