This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS70445 high temperature problem



Hi All,

We are using the dual output regulator TPS70445 in one of our applications and power supplies for this are as below.

1. Input supply : 5V in pints VIN1 and VIN2

2. VOUT1: 3.3 V

3. VOUT2: 1.2 V

It is observed that the temperature of the regulator becomes 70 to 80 deg C once the circuit board is up and running for about 1 to 2 hours. The temperature is measured using IR temperature scanner (non contact type).

Pl let us know if

1. The temperature of 70 to 80 deg C is OK for the regulator to operate safely

2. If not, what are the steps to be taken to reduce this temperature.

Thanks in advance for your time.

Regards,

Jayaram C B