Hi,
I am planning to use TLC5947 in my project. I need to control 20 independent LED's.The datasheet of TLC5947 shows a two wire communication between Microcontroller and TLC( SIN and CLK), but it is not mentioned whether the communication is I2C or not. Kindly confirm the communication protocol used between Microcontroller and TLC.
The current requirement for each led is around 1.5A. I had earlier planned to use a single channel LED current sink driver (ST Micro)with 1.5A capacity.Kindly confirm whether I can use TLC and STMicro driver in cascade(i.e OUT pin of TLC is connected to PWM input of STMicro driver), I know the PWM will become inverted but I can manage that.
Thanks in advance.