Hi all,
I'm working with the TPS54060-Q1 and the TPS54160-Q1 and I'm very suprised of the poor accuracy of the Enable reference voltage : 0,9V < 1,25V < 1,55V. And this is given at 25°C with no indication in the [-40;+85] range.
I'm trying to make a 12V DC/DC which will start when Vin > 12V and will not stop before Vin goes below 16V. Calculating worse cases it seems impossible.
However, on existing boards with TPS54060-Q1, the reference voltage seems close to 1.25.
Any advice ? Should I accept to have my 12V DC/DC that may start when Vin = 8V to be sure that it will still be ON at 16V ?
Thanks.