1.According to wpc, Tx has many kind.The input voltage are 5v,12v,19v and so on. If we design the Rx coil based on 19v TX system.Could the designed Rx coil suitable for 5V,12V Tx system.
2.Could you provide some information about Tx&Rx chip's inner structure (bq500210 or bq500211/212A,bq5101x). And how the chip work? I want to kown how to design the Rx coil to improve the system base on the chip,and the RX coil design is related tightly to the chip. So, could you tell me the detailed information about the Tx &Rx chip.
Thank you!