This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24075T's Vout

Other Parts Discussed in Thread: BQ24075

Dear Tiers.

BQ24075's Vout(Reg) is 5.5V in below condition.

Vin>Vout+Vdo(300mV).

This means when Vin is 6V, Vout is 5.5V. Is it right?

Another question.

If Vin is 5V, Vout is 5V or 5V-Vdo(300mV)=4.7V?