Hi,
I need to switch a resistor at a motor terminals to slow the motor rotation. This resistor has a low-side switch (with PWM command) and a high-side switch with an ON-OFF behaviour. As the HS command can be continuous, I would like to use the TPS2490 as a high-side mosfet driver, taking advantage of its integrated charge pump. But my problem is that the voltage can be as low as 3V, and the TPS2490 won't work with such a low voltage.
My question is : is it possible to disconnect the VCC and Sense pin from the mosfet Vdrain and supply the controller with an unisolated auxiliairy power supply.
Thank you for your help,
Regards