This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5118, 30Vin & 45Vin 24Vout @1.5A

Other Parts Discussed in Thread: LM5118, LM5116, PMP

Hello,

I am new in the hardware development and trying to design an converter(DC-DC), where i have two different input voltages

Vin1 = 30VDC

Vin2 = 45VDC

I used webbench designer to simiulate it and LM5118 was recommended. attached is the schematic.
I want to know, did someone got experience of generating 24V DC@1.5A using LM5118
what do you think about the schematic i attached. Should i go further with the design or are there any other possibilities ?

waiting for your replies :-) 

LM5118.pdf