Hi
We are using LM3642 as a flash LED driver in conjunction with Omnivision OV5645 in flash mode.
As explained in the datasheet, the mode bits are reset once flash time-out period expires.
We don't want to reset mode bits each time the LED is flashed.
For this we tried to set the flash time-out to 800ms and drive strobe signal for 100ms so that the time-out does not expire and the bits are not reset.
But this is not happening, the mode bits are still getting reset.
Please correct if there is some understanding issue.
Thanks