concern about the current sensing input bandwidth of the bq34z100. A/D conversion update is approx. 1sec. The changes in the current could be in the 10's of Hz ( e bike motor controller) and contribute to SOC of the battery. Chip uses a delta sigma for the a/d and is continuously running. Not that familiar with this type, but never seen a sample&hold used with them like with SAR types. Will the bandwidth of the current signals be limited to the conversion rate and lower missing the higher frequency content? or during that 1sec conversion, signals in the 10's of Hz be averaged in the result. Understand that much higher frequencies need to be filtered.