This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TL783 datasheet, figure 14 (current boost configuration)

Other Parts Discussed in Thread: TL783

Hi team,

I'm looking over the figure 14 schematic and trying to get an idea of how the current sharing between the actual regulator and the NPN would work.  My initial thought is that the NPN would be doing all of the "heavy lifting" and supplying the current to the load and the voltage regulation would come from the LDO itself.  That being said, the LDO would only be loaded enough to cause the PNP/NPN chain to bias to supply the required current and then the system would settle under the load (28V,4A)  

What I'm trying to determine is the base current at the PNP but it is understanding the actual load on the LDO at this point of steady-state operation that I'm not quite grasping.  Once I have that, I think I can figure the rest. 

  • Michael,

    In figure 14, the TL783 acts like a shunt regulator. It draws whatever current needed to keep its output voltage constant. This current is about 70mA more (0.7V/10 ohms) than the PNP base current.

    For heavy load PNP base current is IOUT / ([NPN beta] * PNP Beta]) which is a small current.