Please let me know about two point below of SM72295.
・Can SM72295 use Bridgeless PFC?
If SM72295 can use, Is there an application note?
・Is there an application note (or refarence design) of over 1MW power application?
Best regards,
Satoshi
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Please let me know about two point below of SM72295.
・Can SM72295 use Bridgeless PFC?
If SM72295 can use, Is there an application note?
・Is there an application note (or refarence design) of over 1MW power application?
Best regards,
Satoshi
Satoshi,
Apologies for the delay. Your post was not showing up in my queue, but we have resolved that. Thanks for your patience.
The highest power TI Design for brdigeless PFC currently on the web is for a 310W application: http://www.ti.com/tool/PMP9640?keyMatch=null&tisearch=tidesigns-power
This may be of use as a reference for your needs.
How are you planning to use the SM72295 in the bridgeless PFC design? Note that the SM72295 is a dual 100V driver, so the bus voltage at the drain of any high-side FET driven by this part must meet this spec. If the plan is to drive low-side FETs only, we could recommend a more suitable driver if you let us know the MOSFETs used in the design.
Regards,
- Daniel