Hi,
Customer of mine intend to use TPS65261 for AV Receiver application and generated the loop response using WEBENCH based on following condition (see attachment):
Vin = 11V ~ 17V (rated at 14V).TPS65261_Report.pdf
Vo,Io =
1) 5.2V,3A
2) 4.5V,2A
3) 2V,2A
He then found that gain phase margin needs improvement for all channels. It is because the gain/phase margin will become completely out of spec when aging in low temp condition, and might cause DCDC IC shutdown due to reliability and responsibility issue.
Could you advise how to tune the compensator value to have the gain/phase margin as below:
Phase margin = 50 ~ 80 degree, Gain margin = 20 ~ 40 dB.
Thanks!