Hi folks,
I need to syncronize two cascade dc dc converter: first is TPS54340 (output voltage 12V), and second LM22672 (input 12V, output 3v3).
I see in datasheet it's possibile to self syncronize two LM22672, but I cannot find more information about ""output clock"" of the LM22672.
Which is the oscillation frequency when used LM22672 in self sync.?
Is it possible to use in such easy way LM22672 RT/SYNC pin to drive the TPS54340 RT/CLK pin?
Thanks!