Hello,
Please tell me the optimal resister value of RSEN/RSL when I depend on the slope compensation.
<Conditions>
・VIN = 24V
・VOUT = 150V
・IOUT_max = 200m - 300mA
・L = 220uH
It is difficult to determine the RSEN and RSL value because of the variation of VSENS is too large.
Please tell me the recommended value.
In addition, I'd like to know also about the value of CSEN.
Although PMP8956 close to our condition is arranged 1000pF, can I use the same value without worrying about ISEN?
Best Regards,
H.Fujikawa