This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[UCC28950] Reccomended isolated gate-driver for UCC28950

Other Parts Discussed in Thread: UCC28950, UCC28070, UCD3138, UCC28180, UCC28019A

Hi,

I would like to know part number of isolated gate-driver for like a Typical application by datasheet.

If there is no recommended isolated gate-driver, please tell me the point to be aware of in terms of choosing it.

I also see datasheet of UCC28950EVM for reference.

The circuit is another type from typical application on datasheet of UCC28950 ,why this circuit method is different?

I want to know the proper use of two of the circuit system.

In the case of the 1kW about 800W output from using the device, what the PFC is optimum what type?
In the material I found on web ,in the range to 1kW from 800W,  
  Target device is UCC28070.
Dual-Phase CCM Interleaved + Bridgeless CCM PFC had been described as optimal. 
  Target devices are UCC28180,UCD3138,UCC28019A etc.
There is a problem to use Single-Channnel CCM and Dual-Phase TM Interleaved method?

Because we want to as much as possible inexpensive system, choices we believe wide better is a good.
I'm considering configuration of battery charger that input AC voltage range are to 280V from 150V and output DC voltage is 48V.
Please tell me any imformations if there is helpful one.
thanks.