Hi Team,
Our customer would like to use the following conditions.
[conditions]
Vcc=5.0V
Vin=2.1V to 4.2V (1cell)
Vout=1.2V
Iout=around 3A
Could you please let us know if you have any information?
[Q1]
Could you please let us know the VIN current at VCC=0V, VIN=4.2V, EN=0V?
I’m understanding that this value is lower than "10uA".
Because, according to the datasheet, the VCC current is 10uA(max) at VCC=VIN=12V, EN=0V.
[Q2]
According to the datasheet, the recommended range of VIN is “2.0V to 18V".
If VIN is less than 2.0V, Does this device become the unstable behavior?
Regards,
Kanemaru