This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS717xx delay en

I am using the TPS71707 to power a microcontroller and I want to delay the turnon rather than ramping with the input rail.  The easiest way would be with a resistor/capacitor ramp on the EN pin.

 No hysteresis is mentioned in the datasheet for this pin.  Is there any internal protection on this pin so that it will cleanly enable with a slow rising input (order of ms)?  I want to avoid the regulator output chattering as the capacitor voltage slowly rises above the threshold.

Jamie