This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

bq24630: Precharge timer also disabled when TTC is low?

Other Parts Discussed in Thread: BQ24640, BQ24630

Hello,

The safety timer is disabled when the TTC pin is taken low or pulled to VREF. Is the precharge timer also disabled when TTC is low or pulled to VREF? We weren't sure after reading the datasheet.

We have an application where an ultracapacitor module or LiFePO4 battery pack might be connected and the caps could take longer than 30 minutes to reach V-lowv threshold.

If there was a way to lower the V-lowv threshold of 0.35V, that would also help a lot. Down to zero volts would be great.

Thank you!

JohnM