I would like to run a 317 with only 5 ma. of current (240 ohm resistor). I see lots of circuits in the data sheet, but the spec. says 10 ma. minimum or the voltage may rise. I think this is sensitive to the adjust current, and Vin to Vout voltage. The real question is can I do this and is there a way to predict the performance of the IC.
My input is 17 volts. Vout is 3.3 to 12 volts and current is 5ma (from the set resistor) to 0.5 amps.
Thanks for the help