Hi Everybody,
I need to design an interface to an electricity meter that provides a non-isolated 12V DC that could be in reference to either 240AC or Neutral. There is an isolation requirement of 6KV which mean 6mm of clearance and the output I need is ideally 4V @1A but I can also work any voltage up to 12V (4Watts). I am struggling to figure out how to approach this design. I thought I could just use two 2W DC to DC 6KV isolated modules in parallel, but I am not sure if they would work. Any thoughts?
Regards,
Paresh