Hi there,
I'm working with a legacy design which uses a TPS65950 to power an AM3703. However, my board manufacturer is concerned with the part and it is introducing significant complications into the layout.
While I would prefer to work with a part like the TPS65910, I don't have any control over the AM3703's firmware so I can't use this part instead. Does the TPS65950 come in any alternative packages? We have plenty of board area to work with, so a bigger package/pitch would be preferable. I've also noticed that the TPS65951 seems to be quite similar to the TPS65950 - would we be able to migrate to this chip without changing the AM3703's firmware, given that we aren't using any of the features (keypad, etc) which are on the TPS65950 but not the TPS65951?