This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TI TPS61221 replacement for Linear Technology LTC3525-3.3V?

Other Parts Discussed in Thread: TPS61221, TPS61097A-33, TPS61291

We currently make an instrument that uses an LTC3525-3.3V (Linear Technologies) step-up DC/DC converter to generate 3.3V from 2 x AA cells. However, the LTC3525 has become expensive to source in low quantities ($6 for < 500 from digikey and element14) so we are looking for a part to replace it.

The instrument is a data logger designed to run for a very long time. Normally it consumes < 100uA, but there are periodic writes to an SD card which consume up to 100mA for a very short period of time.

The features of the LCT3525 which make it attractive are:

  • 100mA out (max) at 1.25V
  • 7uA quiescent current
  • 92% max efficiency @ 2.4V (85% efficiency @ 0.1mA at 2.4V)
  • Vin > Vout operation up to 4.5V
  • Min Vin once started of 0.5V

Looking at the TI catalog, it seems the TPS61221 or TPS61097A-33 would be good replacements.

  • Are there any other parts I should be looking at?
  • Apart from minimum voltage and quiescent current, is there any difference between these two TI parts?
  • The TPS61097A has MSP430 in its list of applications, any reason why apart from low Iq?
  • What happens during Vin > Vout?